General (Basic LTE FDD PRACH)

The General table in the PRACH carrier node enables you to turn the PRACH carrier on and off, select a saved channel configuration, and set the length of the generated waveform.

The Baseband parameters for the PRACH carrier are described in Baseband (Basic LTE FDD PRACH).

State

Double-click or use the drop-down menu to turn the carrier Off or On.

Channel Configuration

Select a channel configuration with the desired bandwidth and number of resource blocks (RB) from the Closeddrop-down menu.

The User Defined setting is not selectable until certain parameters are changed, then User Defined is automatically set by the software.

Waveform Generation Length

Choice: 1 subframe (1ms) | 1 frame (10 ms) | 2 frames (20ms) | 3 frames (30ms) | 4 frames (40 ms) | 8 frames (80 ms) | 10 frames (100ms) | 11 frames (110ms) | 20 frames (200ms)

Default: 1 frame (10 ms)

Double-click or use the drop down menu to select a waveform generation length. Total Sample Points is based on the selected Waveform Generation Length and Oversampling Ratio as shown below:

Total Sample Points = Base Sampling Rate (MHz) × Oversampling Ratio × 1000 × Waveform Generation Length (ms).

Figure 1 shows PRACH Preamble structure.

Figure 1. PRACH Preamble structure